REGEN.TYPE

Description

You can specify a user-defined external regen resistor or select the internal regen resistor. The values for REGEN.TYPE are shown below:

Type

Option

Description

–1

External Regen

External user-defined regen resistor

0

Internal Regen (if available)

Internal regen resistor

If a user-defined regen resistor is specified, then you must also define this resistor's resistance (REGEN.REXT ), heatup time (REGEN.TEXT), and power (REGEN.WATTEXT).

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

–1 to 0

Default Value

0

Data Type

Integer

See Also

N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

REGEN.TYPE

3007h

03h

Signed8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

2403

1

2403 (0x963)

REGEN.TYPE

Signed8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

REGEN.TYPE

2403

Signed8

Read/Write

-